C Controller Interface Module Features
Q173SCCF
- Features
- Advantages
- Software Development Environment
- SSCNETIII/H
- SSCNETIII/H Head Module
- Positioning Control
- Other Axes Start Function
- Pass Position Interrupt Function
- Tightening & Press-fit Control
- Interface Mode Function
- Functions List
Features
- The system is configured with a C Controller that has a longer product life cycle on the market than the conventional PC.
- Event-driven programs, which use interrupts, can be created.
- Equipped with Positioning functionality using Point table.
- The SSCNETIII/H Head module allows the Interface Module to connect remotely with various modules (I/O, analog, high-speed counter, etc.) via SSCNETIII/H.
- An API library is available for more efficient software development.
- The Interface Module supports C Controllers where Lineo uLinux is installed.
(Note): Contact your local Mitsubishi Electric office.
Advantages Q173SCCF MR-MCseries
Configuration
Software Development Environment Q173SCCF
Create a user program by adding the positioning control API library to the project of the C Controller software development environment "CW Workbench". Since the OS for the C Controller (VxWorks ® ) has been pre-installed, you do not need to install it.
Utility
The utility for C Controller Interface Module/Position Board includes the following software that is necessary for application development.
Test tool
This tool supports parameter and point data settings for application development, operation check such as servo adjustment and error analysis. MR Configurator2 can be started from the test tool, so servo adjustment is easily performed.
Easy test operation check
Test operation is easily performed by using Positioning test operation functions and Parameter/Point data setting functions.
These functions are useful for checking SSCNETIII/H wiring and motor movement.
Maintenance
You can confirm the sampled waveform of monitor data (32 items) and bit data (16 items) to check the sequence of user programs and startup timing.
Error analysis is carried out with ease by reading the alarm history stored on the non-volatile memory.
API library
The API library is the API functions for creating applications for C Controllers or on a personal computer.
Servo amplifier initialization, parameter change, startup in various operation modes, and monitor, etc. are available.
Device driver
The device driver is software required when a C Controller/a personal computer accesses to the Interface Module/Position Board from a user program via PCI Express< ® /PCI bus. You do not have to separately prepare a device driver.
High-speed Synchronous Network SSCNETIII/H Q173SCCF MR-MCseries
- Communications speed is increased to 150 Mbps full duplex (equivalent to 300 Mbps half duplex), three times faster than the conventional speed.
System response is dramatically improved. - Smooth control of a machine is possible using high-speed serial communications with a cycle time of 0.222 ms.
- Synchronous communications are achieved with SSCNETIII/H, offering technical advantages for machines that require deterministic control.
- Long distance wiring is possible up to 3200 m (10498.69 ft.) per system (maximum of 100 m (328.08 ft.) between stations x control axes up to 32 axes), suitable for large-scale systems.
- SSCNETIII/H compatible and SSCNETIII compatible servo amplifiers can be used together.
(The communications speed when SSCNETIII compatible products are used together in the same system: 150 Mbps full duplex)
LJ72MS15 SSCNETIII/H Head Module Q173SCCF MR-MCseries
The SSCNETIII/H Head module allows the controller to connect remotely with various modules (I/O, analog, high-speed counter, etc.) via SSCNETIII/H.
These remotely connected modules serve as the controller's remote stations, transmitting the inputs/outputs.
This results in reduced wiring since the controller receives the I/O and analog I/O signals directly from the servo amplifier side.
- (Note-1): Sensor input/output signals for inspection devices, etc. can be read/written via the Head module.
- (Note-2): Outputs the hand open/close signals.
Positioning Control Q173SCCF MR-MCseries
Positioning operation is performed using the API library in a C language user program.
The operation is started with positioning data from the point data table and waits until an event occurs by interrupts.
Other Axes Start Function Q173SCCF MR-MCseries
This function automatically starts other axes according to its startup condition and its operation pattern.
Tact time of assembly machines, etc. is shortened with this automatic startup via controllers.
Pass Position Interrupt Function Q173SCCF MR-MCseries
During automatic operation, interrupts are outputted when axes pass the specified position.
After that, the corresponding interrupt process of the user program is started.
- High-speed event processing start on host side (OS) is possible based on the servo axis position
- A total of 64 points can be specified for pass position data of all axes
Operation example
- 1. As the axes are moving to P2 from P1, the interrupt occurs.
- 2. The vision camera takes photos of the workpiece according to the interrupts.
- 3. The position data is read.
The vision camera takes photo responding to the interrupts.
Thus by taking photos periodically with interrupts, more accurate position data is available.
Tightening & Press-fit Control Q173SCCF MR-MCseries
The motor can be switched to torque control (tightening & press-fit mode) during positioning without stopping.
Since the current position is controlled even during the tightening & press-fit control, positioning operation based on the absolute position coordinates can be performed smoothly after switching back to positioning control.
Interface Mode Function Q173SCCF MR-MCseries
This standard feature realizes unique control based on a C-language user program using SSCNETIII/H
The interface mode function transmits the position commands received from a user program to servo amplifiers every operation cycle. This allows servo amplifier to be controlled using a user program.
Speed and torque controls are also available in this method.
So, a MR-J4-B can be controlled based on user programs created with your programming know-how of position/speed/torque commands while taking advantage of SSCNETIII/H servo system synchronous network performance.
- The C Controller Interface Module or Position Board controls the SSCNETIII/H processing. This allows the user-program side to focus on information processing, human machine interface, and Motion control.
- A personal computer with a real-time OS can perform fixed-cycle Motion control using interrupts at every operation cycle.
- Thanks to the position command buffers of up to 64 phases, even non-real-time OS (Windows ® only) can perform at 0.22 ms (the fastest rate) cycle command operation; This enables further increase in accuracy in trajectory control.
Functions List
| Standard Mode | Interface Mode | |
|---|---|---|
| Q173SCCF | ||
| Number of control axes | Up to 20 (MR-J4-B) Up to 16 (MR-JE-B) |
The same specification as the standard mode |
| Control cycle[ms] | 0.22ms/0.44ms/0.88ms (Select using parameters.) | |
| Software development environment | CW Workbench/, Wind River Workbench, for the C Controller module, Setting/monitoring tool |
|
| Servo amplifier connection method | SSCNETIII/H | |
| Maximum distance between stations [m(ft.)] | 100(328.08) | |
| Connectable servo amplifier | MR-J4(W)-B | |
| JOG operation | Provided | − |
| Incremental feed | Provided | − |
| Automatic operation | Point table method, 1-axis control, Tightening & press-fit control |
− |
| Linear interpolation | Point table method, Up to 4 axes interpolation (Note-1) | − |
| Home position return method | Dog method, Dog cradle method, Dog front end method, Data set method, Stopper method, Z-phase detection method, Limit switch combined method, Limit switch front end method, Scale home position signal detection method, Scale home position signal detection method 2 |
− |
| Electronic gear | Electronic gear numerator : 1 to 5242879 Electronic gear denominator : 1 to 589823 |
− |
| Speed units | Command unit/min, command unit/s, and r/min | Command unit/min, command unit/s, and r/min (the unit for speed of monitor output) |
| Acceleration/deceleration process | Linear acceleration/deceleration, smoothing filter, start up speed,S-curve acceleration/deceleration (sine acceleration/deceleration) |
− |
| Stop function | Forced stop, Operation stop, Rapid stop | Forced stop |
| Command change | Position change, Speed change, Time constant change | − |
| Application functions | Hardware stroke limit, Software stroke limit, Interlock, Rough match output, Torque limit, Backlash compensation, Position switch, Interference check (Note-1) , Home position search limit, Gain switching, PI-PID switching, Absolute position detection system, Home position return request, Other axes start, Digital input/output, Servo amplifier general input/output, Pass position interrupt, Tandem operation, Mark detection |
Torque limit, Gain switching, PI-PID switching, Absolute position detection system, Digital input/output, Servo amplifier general input/output, Mark detection, Event detection |
| Auxiliary function | Monitor, High speed monitor, Interrupt, Host PC watchdog, Parameter backup, Test mode, Connect/disconnect, Sampling, Log, Alarm history, External forced stop disabled |
|
| Mass [kg] | 0.17 | The same specification as the standard mode |
- (Note-1): Unavailable when the control cycle is 0.22 ms.