MELSEC iQ-F series Quick Start Guide [Ladder language edition] (video)

Quick Start Guide [Ladder language edition] (video)
Program the FX5U CPU module
- (1)Before programming, make the settings in GX Works3 for connecting the PC and FX5U CPU module.
- (2)Try programming.
- Create a program that makes Y0 turn on/off at one second intervals.
- (3)Compile the created program into executable code.
- (4)Write the compiled program to the FX5U CPU module.
- (5)Check that the program operates correctly.
- Reset or cycle power on the FX5U CPU module.
Reset method for FX5U CPU module
|
RESET complete |
Make various settings
- (1)Try setting analog input.
- (2)Try setting analog output.
- (3)Try setting high speed counter.
- (4)Try setting positioning.
- (5)Try setting Ethernet communication.
-
- [1]Try setting parameters.
- In the video for PLC A and B, the only difference is the port number.
PLC A
PLC B
- [2]Try programming.
Security function types
- (1)Security key
- Disables reading and program execution if the keys of the program file, PLC, PC, and copy destination PLC do not match.

- (2)Block password
- Password can be set to individual program blocks, so developers and users can set passwords as required from their standpoint.

- (3)Remote password
- Allows communication access only to people that know the password.

- (4)File password
- Besides the program file, password can also be set to parameters, so settings of individual modules can be protected.