PLC engineering software (MELSEC) GX Works2


Integrated PLC Engineering Software
Ultimate evolution of PLC engineering software
International Standard IEC 61131-3 compliant
Now an easy-to-use engineering software is no surprise.
In addition to its sophisticated usability, the engineering software GX Works2 deploys the global mainstream concepts of “grouping” and “structuring” for fundamental improvement of programming efficiency.
The world-standard engineering style begins with GX Works2.
Improving design and debug efficiency
1Utilizing sample comment saves time to input comments
Provided sample comments can be utilized as comments in projects.

Time for entering device comments are greatly saved by utilizing sample comments.
2Distinguish similar devices without bother
Set a word device comment for each bit to display the contents of the comment on the ladder.


3Easily copy and utilize device comments
Device comments are copied by copying the ladder of the ladder editor between projects.
When copying a ladder onto another program, the device comments in the ladder are also copied.


4Utilize device comments created in other languages
Japanese, Chinese (Simplified and Traditional), and Korean comments can be displayed in GX Works2 English Edition. The function comes useful when working with offices abroad.