Prepared the option for further advanced applications.
By utilizing such as high precision vision sensors or force sensor, it can automate the advanced work that couldn't be done until now.
The R86TB is a new teaching box further evolved from the conventional high-performance teaching box. Even if a computer cannot be brought to the site, one teaching box can handle a series of processes from setup to maintenance, reducing time and cost.
Allows copy and fitting work to be completed in the same way a person would while the force applied to the hand is monitored. Enables necessary work such as fine force adjustments and force detection to be completed.
This compact 3D vision sensor for small robots delivers high-speed, high-accuracy measurements. It performs high-speed picking owing to its unique model-less recognition processing.