Factory Automation
GT SoftGOT2000 enables remote mobile devices to monitor
the status of on-site equipment
the status of on-site equipment

By utilizing Edgecross, it is possible to monitor equipment from multiple manufacturers.
* Can be used with GOT2000 (GT27 / GT25) and GT SoftGOT2000

Advanced technology exhibition of cutting-edge technologies for automation and measurement
The Mitsubishi Electric Group is exhibiting a number of cutting-edge FA solutions and the latest FA equipment at IIFES 2020, which is being held under the theme of “The digital transformation (DX) of the production site, ready to meet the ‘new manufacturing era’.” The details of the exhibits are also available on the Mitsubishi Electric IIFES special website.