Factory Automation

Mitsubishi Electric Fukuyama Works manufactures various electronic devices, some with circuit boards. By using EcoAdvisor it has succeeded in reducing the number of analysis steps by about 90% and improving the efficiency by about 10% per year.
This AI tool helped identify “repair points” that were difficult to find manually, and helped improve production.





Advanced technology exhibition of cutting-edge technologies for automation and measurement
The Mitsubishi Electric Group is exhibiting a number of cutting-edge FA solutions and the latest FA equipment at IIFES 2020, which is being held under the theme of “The digital transformation (DX) of the production site, ready to meet the ‘new manufacturing era’.” The details of the exhibits are also available on the Mitsubishi Electric IIFES special website.