质量和环境

ISO9001

High frequency and optical device work has received ISO9001 certification for our quality management system which supports our operation to supply high quality products.

Business unit Certification Authority Certificate NO.
  • Optical Device Business
  • High Frequency Device Business
  • Infrared Sensor Business
LRQA ISO9001-0066600
SiRF Device Business LRQA ISO9001-00015476

For more information, please click the Inquiry button.

The Restriction of the use of certain Hazardous Substances

红外传感器符合RoHS指令(2011/65/EU、(EU)2015/863)

RoHS : Restriction of the use of certain Hazardous Substances in Electrical and Electronic Equipment