Information and communication systems Transportation control system/Operation control system
go to Transportation control system
The Train Operation Management System (hereinafter referred to as TOMS) is the system that
supervises and controls the train operation intensively. The TOMS of MITSUBISHI has the following
characteristics.
  • The Optimum System Configuration for Route Conditions and Train Operation
    Regardless of the route scale (large or small), the TOMS supports the centralized system, the distribution system, and the integrated system configuration of both systems.

  • High Degree of Confidence, Expandability, and Flexibility
    The TOMS realizes high degree of confidence and expandability of the system by multiplying the equipment and the networks.

  • Realization of User-Friendly Interface
    The effective supervision of CRTs and projectors and the unified user-interface have improved the operability, viewability, and response performance of the system.

  • Adoption of the Universal System
    Adopting the general-purpose standard OS and networks has given the TOMS high expandability.




back to top