Information and communication systems Inspection system/Wheel shape measurement system
go to Inspection system

The Wheel Shape Measurement System (hereinafter referred to as the System) is the equipment that automatically measure the diameter and thickness of tyres, height, thickness and angle of flanges, and vertical wear of flange without touching them. The Detection Section, which is installed on the track, with buit-in laser light sources and CCD cameras takes photographs of the passing wheels. The Data Input Management Section beside the rail image-processes the photographs and automatically calculates the measurements of each part of the wheels. The calculated measured values are sent to the personal computer (PC) in the office. The PC displays, prints out, and manages those values. In addition the PC shows the photographed images so that the wheel profiles can be monitored. The System exchanges data with upstream data management systems and the wheel lathe unit with the aid of the Ethernet.

Detection Section
Data management section
Image Display
Transition graph of wheel wear
History data of wheel dimension
back to top