- Space Systems
FOR IMMEDIATE RELEASE No. 3216
TOKYO, October 9, 2018 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will release a compact version of its mobile mapping system (MMS) on December 25. MMS are highly precise measuring systems comprising car-mounted GPS antennas, laser scanners and cameras to gather 3D positioning data on road surfaces and roadside features, generally used as base data to create high-definition 3D maps for autonomous driving and infrastructure inspections. The compact, lightweight and transportable new MMS-G, which is especially suited to mounting on automobiles, railways, carts or ships, is expected to be used for diverse applications in markets including Europe, North America, Asia and Oceania, where high growth is forecast.
The new MMS-G will be showcased at the Mitsubishi Electric stand, No. 12.1E.080 in hall 12.1 during INTERGEO at Messe Frankfurt exhibition complex in Frankfurt, Germany from October 16 to 18, 2018.

Product Features
- 1) Compact, lightweight model for easy transportation and diverse installations
- Compact design integrates three Global Navigation Satellite System (GNSS) antennas into one to reduce weight by about 50% compared to existing MMS-G220Z model.
- Roof-mount unit divides into two units for easier transportation/installation and reduced labor.
- Diverse mounting on not only automobiles but also railcars, carts, ships, etc.
- 2) Diverse, high-precision field surveys for 3D mapping and infrastructure inspections
- Inertial measurement unit (IMU; for detecting position, velocity, attitude and heading) and speed sensor can be used where satellite signals cannot be received, such as tunnels.
- High-sensitivity camera enables data acquisition at night.
- 3) Simple operation does not require specialized training
- Unique, proprietary operating software and GUI enable field surveys to be performed without complicated settings.
- Estimated measurement accuracy can be confirmed on operating screen in real time, enabling users to select operations efficiently for optimized data acquisition.
- Obtained data can be used to construct 3D laser point clouds easily with post-processing software (provided).
Future Application
Mitsubishi Electric is developing markets in Europe, North America, Asia and Oceania, where the demand for highly accurate, precise and efficient field surveys and infrastructure inspections is expected to grow. Demand is especially promising in North America and Europe, where high-definition 3D maps are required as base data for autonomous-driving demonstrations currently under way and envisioned commercial systems in the future.
Mitsubishi Electric's new MMS-G, in addition to field surveys and data acquisition for autonomous-driving maps, can be flexibly mounted to inspect railroads, coastal embankments, hard-to-access areas and more. It is expected to be used widely, and thereby expand Mitsubishi Electric's global business in this field.
Inquiry
Media contact
Customer Inquiries
Related articles
- Space Systems
-
Nov 29, 2024
-
Oct 02, 2024
-
Sep 19, 2024